mappView camera scaling

Hi Jose,

Do you want to show the results from the Vision Function as animation or do you want to show only the image?

In the Paper Widget, if you want to used the parameter Select, you need a SVG File. It is the ID of your SVG Image, here in the documentation, you can find more information about it Paper Widget

For example in my Content I added a Paper Widget with my Limits.svg file. It contains two lines LimHigh and LimLow:
image
In the transform string, I sent the values, where it is going to translate the line, OffsetLimitStr := ‘[{“select”:“#LimHigh”,“duration”:0,“translate”:[0,0 ]}]’ :


If you want to deactive the zoom in / out the value should be 100 in max / minZoomLevel.
Probably you have to scale the translate values to fit with your image :wink:

But if you want to show only the image from the camera, I would recommend you to use the Image Widget, where the Imagepath, it is the actual image from the camera. You can find more info here
The sizeMode parameter as Contain, it going to fit the image in your layout.

I hope, it would help you.