hi, i have a 4pp32p panel and the board is broken, also have a 5pp320 panel but no boot with the 4pp320 CF card, starts to boot but i have a bluen screen, what can i do?
Windows blue screen? So Windows crashes with some error? Or is it a screen with AR startup? What is then on this screen? Run, Service,..?
Thanks in advance, is a AR startup blue screen, only blue with cursor, CF boots ok with old 4PP320 panel (thats broke board touch conector)
Ok, with the AR system, you can exchange the CF card from one panel to another one ONLY if the panels are the same. Otherwise, it will not start. So the behavior is as expected. If you do not have the source project to change the hardware, you would need to get in contact with the B&R repair department. But I’m not sure if this old hardware can still be repaired. This must be clarified with them.
thanks, i need a 4pp320 board…
sorry that I can not help you more.