Modbus Register Addressing for variables

Hi,

if I got it right and you’re using modbus serial on one of the “normal” serial interfaces of the PLC, then the’re no address assign by tag editors.
In that case, the Modbus RTU protocol is processed by own code using library “DRV_mbus”.

How to put/get modbus data (coils, registers) into process variables depends on if you’re a modbus master or a slave.

  • Being a master, the configuration is done by settings in the configuration data module that has to be used together with the function block “MBMOpen” - in this module, existing process variables are “linked” to modbus coil or register addresses
  • Being a slave, the “coil or register memory” is linked to process variable arrays either by providing the addresses of the arrays when calling the function block “MBSOpen”, or by declaring global array variables namens “MB0[i]” … to “MB4[i]” (for the 4 different modbus variable types) with a suitable array size to cover the whole register range you need to use. This varables then are automatically used by MBSOpen.

So if the modbus communication is already established, I assume you already have some running code based on the DRV_mbus library: is it a master or slave?

Best regards!