I am experiencing an ODBC Microsoft Access Driver Login Failed error in Automation Studio when adding a blank ST-Program All In One to the existing project.
When I click on “OK”, this window shows up:
When I click on “Database…”, this window shows up:
When I click on “OK”, I’ve got the same “Not a valid password” error.
When I click on “Cancel”, I’ve got a low memory error, but I have plenty of RAM available.
However, the blank ST All in one program was added successfully and I was able to compile the project successfully. B&R support engineer believes the issue is Windows 11 and a Windows re-installation might be required.
I also have Automation Studio 6.5 installed on the same laptop and I did not have any error when adding a new program in Automation Studio.
I am running AS 4.12.9.18 and here is my runtime versions:
Thanks,