Hi,
I am trying to establish a secure OPC UA connection between a B&R OPC UA Server (Automation Studio 6.5.1.7) and a Siemens S7-1500 OPC UA Client using Sign & Encrypt.
Communication without security works correctly.
However, when I connect from the Siemens PLC, the connection is established briefly and then immediately disconnects.
On the B&R side I configured the following:
⢠Picture 1: Under Certificate Store Configuration I selected SSL Configuration. The B&R server uses a self-created server certificate and private key.
⢠Picture 2: In the SSL configuration, the B&R server certificate is configured as the own certificate. Under Trusted certificates I imported the Siemens PLC client certificate.
I followed the steps from an existing B&R Community post (@UAExpert, mappView: How to make a secure OPCUA connection to OPCUA server with communication partner validation) about configuring certificates, so I believe the certificate setup should be correct.
Is there anything else that has to be configured for secure communication with a Siemens OPC UA client?
Thanks in advance!