Hi all,
from time to time I need to ping a device from the PLC, for example in test setups a.s.o.
Therefore, for my own convinience, I coded a small library that exposes the ping functionality to a small web frontend (not nice, but functional
) that helps using ping like in routers or other embedded devices.
Additionally, some statistic values from a ethernet interface can be shown.
Here, I want to share this with you, maybe anyone else can somewhen utilize it, who knows?
It should be easy to use:
-
import the library “WebPing”
EDIT: I removed the download , the library can be found inside my Github repository, pls. see the infos in the following post -
execute the function block “webPingInterface” in a task
-
That’s it.
If everything is ok, you should now be able to open “<PLC’s_IP_address>/ping.cgi” in a browser and see the frontend.
(internally, the function block uses the capabilities from the B&R Libraries AsICMP, AsHttp, AsETH, AsArCfg, AsHost to collect and provide the information shown in the web frontend).
Here’s a short description for the frontend:
Output when ping was successful:
Output when ping failed:
Output of statistic values of the PLC’s ethernet interface: