Scan network SNMP from terminal/CLI

Hi,

i already started linking brsnmp with the PVI6 lib/dll.

I did not publish it yet since we face an issue with PVI6.x (QCAS-4517) which will be solved in PVI 6.5.2.

On the other hand there is no disadvantage in using brsnmp with PVI4 in combination with AR6, I don’t see any restrictions.

Unfortunately, SNMP is often disabled on controllers based on AR6, as this is the default setting for AS6.

It may therefore be necessary to rely more on the ANSL line in the future.

+++

Many IT administrators get nervous when unfamiliar *.exe files are used.
In another post, I showed that a combination of sockets and ANSL can also be used to perform a network scan using Python.

1 Like