Teltonika Router For Remote PLC Connection

Does anyone was successful connecting to a B&R PLC with Teltonika VPN Routers.

When adding a VPN route in the Teltonika configuration, the Router goes into scanning mode of the network, somehow all devices appear but the B&R PLC.

I have tried adding the route manually, which is possible, but it seems that something blocks the connection to the PLC, I don’t if it comes from the Router or the Panel PC.

Any help would be appreciated

Question to AI:
How can we connect B&R PLC with Teltonika VPN Router?

Answer:

Video

AI should be our big brother soon, we will see…
Thanks
Ciao
Valerio

To add to Valerio’s response, there is a list of ports used by different features in the Help. The default TCP port used for ANSL communication (connection between Automation Studio and the PLC) is 11169, so that port will need to be open if you plan to connect with Automation Studio. The others you can block/unblock depending on what you plan to do with the connection.

If you look at the attached picture there is no Gateway Parameters available

Hi,

the default gateway is a system-wide setting that can be configured via the CPU configuration:
https://help.br-automation.com/#/en/4/projectmanagement/systemconfiguration/sg4/cpu/projectorganisation_systemconfiguration_sg4_cpu_ethernet.html

Best regards!

@David_Vieira

small note (not related to the post) about point 2) You are using new hw but you have configured an old 1.1.0.0 hw upgrade, the latest one 1.2.1 introduces the support for multicore load balancing. Just let you know in case you need that feature you have to select 1.2.1.0 hw upgrade:

Ciao
Valerio

Thanks Valerio and Alexander, still have the same issue, start to think it is a parameter in the router. I will put a call in tomorrow with Teltonika to see if we can resolve the issue.

For some reason I can’t explain, the issue came from Teltonika subnet setup. Like you see in the picture, PLC ip:192.168.1.10, PLC subnet: 255.255.255.0.

Teltonika Subnet had to be set to 255.255.255.255

Thanks guys for your help

Spettacolo! Thanks for the feedback.
Please mark your comment as solution.
Ciao
Valerio