After using the help files to migrate my AsOpcUac library from AS 4.12 to AS 6.0, I was able to transfer the application to the target. However, the UA_MonitoredItemAddList function block gives me an error code 2952790020 for invalid variable names. The variable names did not changed and they are working for AS 4.12. I double check the required syntax for the variable and my syntax is correct. I am not sure what else could cause this error. This application is downloaded to a OPC client target and it looks like the issue is coming from the client. I used UAExpert to check the OPC UA server side and it is working correctly.
I enable the OPC UA client/server but I did not enable the variables on the client side. I did not have to in AS 4.12. Do I need to do it in AS 6.5?
With the suggested solution of providing NodeQualityID, i was also able to fix the variable issue.
How ever after that in the UA_MonitoredItemOperateList function block i get node error - 16#807B_0000 / 2155544576 which i am not getting how to resolve,
I have set the subscription timeout as 1m, publishing interval 1s and monitoring for variables is 200ms