Unkown task in task class 4 profiler runtime 6.2.1 Svc#4.255

Has enybody a idee whta this tasks is ? all create programmed tasks are accounted for.

Best regards Wouter

Hello and welcome !

“unknown tasks” may appear if tasks are created during runtime by libraries, mapp components or the OPC UA server. These tasks are not defined in your configuration but are generated by the system during execution

best regards
Oliver

Oliver is right as usual :wink: More info about same topic here: When analyzing the program using AS's profiler, the unknowncylic task appears