Ups-daemon question for install


when I use debain12 could I install ups-control?
ups-control depends on daemon ,but Deamon don’t have package for Linux Debian 12,
I try to install ups-darmon_1.2.4 on Debian 12.
when I install it ,there has an error like the picture.
Customers need this libbrad2 package for installing ups-daemon, but I can’t find this package on linux.com.
Is this package developed by us?
I have searched the official website, but I can’t find it.

Hi @mar,

as I remember, libbradi2 is part of the following package:
https://www.br-automation.com/en/downloads/software/operating-systems/linux-for-br-10/adi-library-linux-for-br-10/

This package can only be seen/downloaded if you’re logged in at the homepage.
I think also the mtcx package is needed (same location on the website).

But be aware that these packages were built for B&R Linux 10 based on Debian 10, I don’t know if they’re all comaptible with Debian 12?
Linux for B&R based on Debian 12 is in preparation as I know, but I’m not aware of the release date.

Best regards!

Thank you so much!!!
it‘s very helpful !!

Hi,
I’m happy that I could help!

Best regards!