Hello,
I need to read some process variables from an old B&R controller for diagnostic purposes. Target details:
CPU: Power Panel 5PP520.1214-K04
Automation Runtime version: R4.02 (discontinued)
Network: reachable via TCP/IP, ANSL port 11169 is open and I can establish a Connection
Using the current PVI Development Setup 6.7.0.39 via Runtime Utility Center, the Connection command succeeds, but every variable-related command (TaskList, ModuleList, VariableListGlobal, ReadVariable) fails with:
“Command is not supported for discontinued Automation Runtime version R4.02.”
From the community wiki I understand ANSL is only supported/recommended for AR >= V4.08, and that older controllers should be accessed via the legacy INA protocol instead, which is supported by PVI 4.x.
However, the public Downloads page (Category: Automation NET/PVI) currently only lists PVI Development Setup 6.7.0.39 - no older 4.x versions are available for download, even with All Versions selected.
Could someone point me to where I can get an older PVI Development Setup (ideally 4.1.12, matching AS4.1.17.113) that supports INA? I don’t have the original Automation Studio project for this machine, so PVI is the only tool I have to browse the variable list.
Thanks in advance!