7cp470.60-1 cpu uploading program

Hello, Im new in this forum

I have CP470 cpu on working machine, is there any way for uploading a program from plc and downloading to other one ?

thanks

Hello and welcome,

You cannot upload the source code but you can upload the binary content

Here is a howTo you can follow:

HowToBackupSG3Targets_eng_AT.pdf (1,0 MB)

Please note that the binary content cannot be modified - if you would need the original source code you have to reach out to the machine manufacturer

best regards

Oliver

Hi Khaled,

may be this brochure helps.

HowToBackupSG3Targets.pdf (1004.4 KB)

Regards, Torsten

Thank you fo help, is there any way to uploading a software for this operation ? like AS 2.7 or other tool

When you take a look at the PDF there are basically 2 ways to do an upload:

  1. Using PVI Transfer tool (which is part of PVI setup)

  2. Using Automation Studio (like AS2.7) and PVI transfer tool

You will find PVI and also AS2.7 on our homepage:

Automation Studio V2.7 | B&R Industrial Automation

PVI Development Setup | B&R Industrial Automation

If im correct it’s rs232 communication cable for connecting to plc, please send me if posible a wiring diag. for it.

Thanks

The RS232 cable is also mentioned on our homepage:
Datasheet RS232 cable | B&R Industrial Automationation

And this is the Pin layout:

Probably you might also find the system 2003 manual useful:

System 2003 User´s Manual | B&R Industrial Automation

Your CP470 is a so called system 2003 PLC

hi @HKTEC, what is the status of your topic? can you update us?

Hello,

I’m waiting for the machine supplier to send me the PLC program.

ok. if you need additional help, do not hesitate to continue with discussion, otherwise please mark reply that helped you the most as a solution. Thanks :slight_smile:

Hello,

Thank you for your help. It turns out the problem is with the CPU; we need to replace it.