Configuring Limit Switch for ACP10 using the 8EAC0130 card is not as comfortable as for mapp motion.
If I have a configuration like in this picture :
Then I would like to assign DI3 and DI4 to work as POS_LIMIT_SWITCH and NEG_LIMIT_SWICH.
So in this case it will correspond to (5665; DIO_IN3+1) and (5673; DIO_IN4+1).
( Slot 1 is always used on the 8EAC013x.000-1 )
I can read the values in the Test window as a check.
And then I simply assign these DIs to the table :