Accesing data from X20CP0291 using raspberry pi with OPC UA server inside

Hi,

you can use more then one instance of UDP communication by using AsUdp, so yes it’s possible to communicate to multiple remote hosts by direct addressing their IP addresses/hostnames.

As Udp is a protocol without flow-control, it should be even possible to communicate via the same socket / port on the receiver, but this would make the data assignment maybe a bit more complex. So if there’s no mandatory reason to do so, I would prefer to use different sockets/ports at the receiver to have a direct 1:1 assignment between the communication partners.

Best regards!