Hi, when I compile and load the program, it goes to the plc service. When I look at the registry, it directs me to this. I’ve defined the values MpAxisBasic[0..7] and MpAxisBasicParType[0..7] as global and will use them as references for local access, but it goes to the plc service.
The ACCESS must be done in the cylic part of the task.
I didn’t fully understand, could you give some details, where should I define the paxARM ACCESS ADR() function?
-Action ‘Accestion’
End_Action-
I enabled it on the main blog,
Accestion();
I have configured this in the cyclical part of the ACCESS main blog
If your action “Accestion” in call in a CYCLIC it should work, one thing I didn’t understand is that you but it in an action it’s for reusability? Why did the index “gARM“ is a constant?
pAxARM ACCESS ADR(gAxisBasic[gARM]); must be called before the pAxARM variable is used by anything else. So your ACTION Accesstion must be the first thing called in your CYCLIC code for the task.
PROGRAM _CYCLIC
Accesstion; (*Call the action to initialize the variables*)
pAxPar.Axis := ADR(gAxis01); (*Now i can start using the referenced function block after it is pointed to an actual structure*)
PAxPar.Mplink := ADR(gAxisBasic01);