ACOPOS and AC112 firmwares

Thanks so much Michael for your clarification on the limitation of old AC112 powerlink card, it supports only V1 mode:
We upgraded a big machine last year and a last minute surprise was the powerlink card mounted on the panel didn’t support the old powerlink mode V1.
After that in our check list o the top we have “check Powerlink mode compatibility“

Second limitation of AC112: you can’t installed latest ACP10 version on that:
Few details I got from Support last year:
”when the customer has a machine which is using a combination of AC112 and AC114 then they need to use PLK V1 and need to stay on ACP10 V2.xx.x versions otherwise AC112 won’t work anymore. The latest version in the ACP10 V2.xx.x family is V2.52.8 indeed. This is “so far” away from V3.xx.x because we simply made a version jump with ACOPOS P3 to V3.xx.x Similar to the jump we made from ACP10 V3.18.2 to V5.xx.x and the jump we are going to make from V5.27.x to V6.xx.x”
Thanks
Ciao
Valerio

3 Likes