Thanks for your feedback.
Here is the status :
- Project and AD are changed to LDAPS port 636, connection is established.
- Certificate of the server was properly generated by IT department of the factory.
- Certificate have the same name in the project and on the server.
- We are using SAMAccountName on the server.
- Mappview is using mappUserX to authenticate.
- MpServer librarie is added in the project.
- Timeclock is synchronized with NTP server of the factory.
- There is nothing running on the project only AD and the login widget.
I still have error when I try to login on mappview using Active directory account –> BnR logger : Error establishing the connection to MpUserX. -1061091324
If I try to login using local user, it’s working well.
The AD sees incomplete request from the application meaning that communication is properly established but something is missing.
Should I fill somewhere as DN base the path to look for users in the AD ? How can I get additionnal informations about diagnostic ? Can it be the size of the frame ? How can I see what is sent to AD ? Can I configure project using only fixed IP address from the server ? (FYI I tried with DHCP and I same error).
Thanks,
Emilie