[APROL4.4] How to migrate CAE database from Aprol4.2 to Aprol4.4

Hello,

I would know if there is a documentation or a procedure for a migration from an APROL 4.2-06 to an APROL 4.4-01 ? Did i need to upgrade to 4.2-07 before ?
If it’s the case, what happened if an APROL 4.2-06 crashed and i have the backup, i need to fresh install a 4.2-07 to convert the backup and after install the 4.4-01 ?
I tried to CAE Restore the CAE Backup from 4.2-06 but it seems that it break the 389DS.

Thanks.

Hello @Vincent_Druart,
to upgrade to APROL 4.4, it is only possible from APROL 4.2-07.
I am including files regarding the update from 4.2-07 to 4.4, and LDAP as well.

If you have a backup from APROL 4.2-06, you are able to restore it in 4.2-07. Then the restored CAE database will be updated to version 4.2-07.
Then you have to make a backup again, and use this backup in 4.4-01.

Update CAE Database from Release R4.0-00 - R4.2-07 to R4.4-01.pdf (802.3 KB)
LDAP.pdf (75.3 KB)
APROL_R4.4.01_LDAP_draft.pptx (4.9 MB)
LDAP_389DS in APROL R4.4-01.pdf (1.7 MB)

Related articles:
B&R help - APROL 4.4 Upgrade notes
B&R help - APROL 4.4 System manual

I hope it will help.

Thank you for answer, clear and precise.

Thanks for the feedback. @tomas.miculka is awesome, I know :slight_smile: