I’m currently migrating a project from APROL 4.2-06 to APROL 4.4-65.
Cae Backup and Restore is fine, i have some blocks modification to do but nothing big.
My problem is on Automation Studio. How can i migrate my 6 controlers from AS 4.8 to AS 6.5 ? i did not find anything about that on documentation.
Did i need to install 4.8 and 6.5 on my pc, export each project, convert it on my pc and export it back to aprol ? Is it the best and efficient way ?
Thanks for your reply.
I know that some types of PLCs are not supported, mines are good (X20CP3687X).
The message is here because on the VM i only have AS 6.5.
It’s a very APROL related question, I already see some scripts to do the conversion inside Toolkits of this community but I want to be sure that APROL authorize this or to know the correct way to do this.
I don’t know how an AS project is the same inside an APROL project or not.
To migrate the controller part of an APROL project to AS 6.5, AS Version 4.12 or later is required.
AS Version 4.12 was introduced with APROL R4.2-07.
As a general recommendation, major APROL project upgrades should be performed from the latest available service release, which in this case is R4.2-07.
Therefore, I would recommend first upgrading the project to R4.2-07 before proceeding with the migration to the new major release R4.4. This should provide the best chance for a smooth and successful migration.
Please let me know if you need any additional information or support during the upgrade process.