AsGuard Dongle read/write

Hello Community,

I want to use the SafeGuard Dongle to store some protected data as machine options.
To do this i would like to develop an executable in C or C++ to read/write the dongle directly on the GPOS, i use an APC 4100 with hypervisor.

I searched on Help and don’t find how to do this, is anyone know if it’s possible or if a driver exist to read/write on SafeGuard Dongle ?

Best regards,
Kevin

Hi there,

The safe key’s sole purpose is to manage the safety application and underlying data. It’s not meant to be user-accessible or a general purpose memory and I am not aware of any means to access it besides via the Safe designer and the libraries (SfDomain for mappSafety, AsSafety for Safety Release).
If you want to store user data, you can always store it on a user partition of your PLC memory (the CF) or an extra USB stick.

Hope that helps

1 Like

If you have a tech guard device (0TG1000.02 | B&R Industrial Automation, , or 0TGF016.01 | B&R Industrial Automation), you can use the AsGuard library to read and write to the 241 bytes of application storage. The 0TGF016.01 also gives you 16 GB of datat storage and I believe should fit in the APC4100’s internal usb port ( B&R Online Help).

You could also use the X20CMR modules, they have 512 kB of Flash, I believe you use Flatstream mode to access, so it isn’t fast storage, or file based storage, but it isn’t easy for users to get to and mess with.

The X20CMR100/X20CMR111 also have the 241kB of tech guard storage via AsGuard. The Tech Guard functionality only works when on the direct X2X bus of the PLC, not behind a bus controller.

Depending on what protected data you are trying to store, and if it is safety related, you could also use the SafeCommission options/SafeTables to store data. This would be stored on the Safe Dongle when it’s loaded on to it and exist through power cycles.

1 Like

Hi @Kevin, what is status of your topic? Can you update us and marked reply that helped you the most?

Hi,

The 0TGF016.01 match with the application, dongle is too limited to do that.

Thanks all for your answers