Automation Studio V2.2

Hi community!
Has anybody installation for Automation Studio V2.2 or higher? And is willing to share it? I need to open and download old project made for PP41 (4P3040.01-490). From project.ini file I can guess it was made for it (StandardDir=C:..\BR_AS_220_L049\as\library\V0230)..

Thanks, Matjaz

Automation studio 2.7 can be found here on the B&R website.

Automation Studio V2.7 | B&R Industrial Automation (br-automation.com)

Support for the licensing servers went away some time ago. I believe if you install this and service pack 18 it will not require a license.

V2.7 AS Upgrade (2.7.0.25_SP18) | B&R Industrial Automation (br-automation.com)

In AS V2.5 the current i/o mapping is introduced, so you have to remove the old copy tasks and mapp the variables.

I will upload it and send download link to your email.

Hello Jaroslav,
We have tried with version 2.2, but it seems aplication was done in it but with some upgrades on basic V2.2 version… Is it possible to get V2.3 as well? I have V2.7 but in one reply of this case it was written that after version V2.5 we have to change some things in the project. I would like to avoid these project changes…

In the zip file I provided to you was upgrade to SP2 of AS2.2. In fact with this service package installation you should have the latest version of AS2.2. Did you install it as well?

Hello
I am newbie for this B&R Community.
I need AS 2.29 to open my project and transfer to New PP41.

PVersion V 2.2.1.0001 Automation Studio 06/26/01 11:23:32
11/12/02 16:08:09 V2.29 PP41 UV
I copy from GDM file
Please send download link to me kai.i98@gmail.com
if possible could i have download link for AS2.4 AS2.2 too?
I can not DM to you 'cause newbie.
Thanks and regards,
Ariyatuch P.

Hi, The download link has been sent to your email. Please note that AS 2.2 and AS 2.4 are not supported and cannot be registered. Therefore, if you need to maintain your project, I strongly recommend updating it to a newer version of AS. Have a nice day. Jaroslav

Hello,

Could you share me the downloadfiles for B&R AS2.4 AS2.2 too?
I’m trying to open an old PP41 program files (.pgp file) and I can’t find find the software anywhere.

Kind regards,
R. Jamin
R.jamin@kpnmail.nl

Thanks so much for your kindly help.

Hello,
i have need Automation Studio V2.2 if you can send it please
to amhaouach.said@gmail.com
thanks