Automation Studio 2.4 Download Link

Does anyone have the Automation Studio 2.4 Download Link? I’m having trouble using version 2.7. thanks!

Hi Rodrigo,

Please see this earlier post: Automation studio 2.4,where to download? - Ask Questions - B&R Community

It is recommended to stay with version 2.7, or upgrade your project to a more recent version (e.g. AS 4 or 6) if you have the bandwidth to do so.

What problems are you having with 2.7? Maybe someone here can help.

Hi Marcus,

Yes, we have alreadey tried to donwload the project using version 2.7. It seems correct, but some functions are missing and unfortunately the machine supplier says that could only works with the version 2.4. We reaaly need this version.

Since AS V2.5 or higher the current i/o mapping is introduced.
This means that the correct variables have to be assigned to the new i/o mapping.
The input and output (iq) tasks have to be removed from the software.
Some data object which describes the old i/o mapping have to be removed.

What other issues do you have?

We have replaced the CPU 7CP474.60-1 at our machine, downloaded the software sent by machine supplier (created on AS V2.4) with AS V2.7, but the main HMI buttons functions doesn’t work properly. It seems to be related to i/o mapping mentioned by you. Thats why we would like to have the AS V2.4, to avoid the changes, if its possible.