Automation studio 2.4,where to download?

I need AS2.4 software because I need to open a project created in this version.
If anyone still has it and can email me at alex@tecjac.com.br

Hi, I will sent you download link to your email address. Check it out.

AS2.4 cannot be licenced any longer
Due to this I strongly suggest to use AS2.7 (which is free of any licence) - the project will be upgraded but as mentioned AS2.4 is in my opinion no option here

Thank you very much, I’ll be waiting.

I’m really having problems, I’m going to have to install Windows XP, or in Automation 2.7 it asks for an upgrade with V2.33 to be able to open the project.

Or upgrade with AR:V2.33

AS2.4 is really old and will not run on Win 7 or newer. This version was released in the year 2004 which means it is 20 years old

AS2.7 is also old but at least it runs on Win 7

V2.33 is an operating system for also old PLCs and I can providethis to you.
Will send it to you via a private message

I thank you because my client is desperate.

Hi Alex, have you got the AS V2.4 software? I also need it for a really old project.
Can you also send me a copy?

HI Jaroslav,
Can you please also send me the download link?
My email is xcc521@hotmail.com
Thank you

yes, I can send you. But please take into consideration this post from Oliver Automation studio 2.4,where to download? - #3 by oliver.doberer. Because he is completely right.

yes please send me the link to xcc521@hotmail.com.
I have installed version 2.7.0, but I cannot upgrade the project from Ver. 2.4.0 as it has an 8AC140.60-1 card that is not supported by later version. So I got stuck.
Thanks Jaroslav.

I sent you download link.

Thanks a lot. I downloaded it and installed it. It worked with my project. :100:

Hi, Jaroslav Kovar, i read the thread, can you send me the download Link for the Automation Studio 2.4. I need open a Proyect with this version. My email is Clquintanilla97@gmail.com

I would be grateful for your Help!!

Greetings!

Download link was sent to your email.

Thank you!!! It was very useful!. I downloaded it

Hi, Jaroslav Kovar, can you send me the download Link for the Automation Studio 2.4. I need to open a Proyect with this version. My email is relettrico@fiorinint.it
I would be grateful for your Help!!
Thanks in advance.

I closed this topic today. If anyone need download link, just send me private message here in community. Jaroslav