AS2.4 where to download for a new user with level 0?)

Hi!

Have a problem with my project, can’t upgrade it. Need to AS2.4, can anyone help with it?

Hi Soslan, and welcome to the Community!

Automation Studio 2.4 is available to download from the B&R website: Automation Studio Upgrade | B&R Industrial Automation

However, this software is quite old now. It was made to work with Windows XP and cannot be licensed anymore. Unless you a way to install and license it, I highly recommend upgrading your project to at least Automation Studio version 2.7.

Hi, @marcusbnr

Service pack needed, i mean. With upgrade still not working, can’t to upgrade and fw error

It looks like you’re trying to open the project with AS version 3.0.90. I recommend installing AS version 2.7 from the link above and then opening the project with that.

The project will automatically upgrade itself when it is opened. Just to be safe, it’s a good idea to keep a backup of the project before the upgrade, or even better to use a version control system (e.g. Git) to monitor the changes.

Thank you @marcusbnr i’ll try

Hi, still not working too different fw. Hope to take as2.4 :smiling_face_with_tear::sweat_smile:

An installer can be provided by official support. But it is not possible to activate it, and you will also not get any support. This must always be taken into consideration. So it is up to you. We recommend updating. :slight_smile: The topic is marked as solved because @Skochiev already asked for an installer.