B&R Automation Studio 6 installation network interface bug

Hello,

I noticed an unusual behavior that I can’t fully understand and would like to report it.

I tried installing Automation Studio 6 (latest version 6.5.1.7) on a Windows 11 virtual machine running on VMware Fusion Pro on macOS Tahoe with Apple Silicon (so Windows 11 is ARM-based).

At the end of the Automation Studio installation, the Windows virtual machine’s network interface stops working properly (I can see it, but it cannot access the internet).

At first, I didn’t connect the Automation Studio installation to this issue. I tried everything I could think of to “revive” the network adapter, unfortunately without success.

I then performed a clean reinstall of Windows, and the very first thing I did after installation was install Automation Studio again. As soon as the installation completed, the previously working network interface stopped functioning once more.

I can’t understand why this is happening. Has this ever happened to anyone else? Which installation component could have broken the network interface?

Thanks in advance for your replies.

Hello,

Doesn’t the following Community topic solve your issue?