C80 PLC not communicating with Wago Network Switch

Hi,
I tried to connect C80 PLC with a network switch. On that time it is not communicating with that network switch(Indication on network switch and PLC is not blinking and connected my laptop to network switch and pinged). When im connecting laptop to network switch, the port indication on network switch and laptop is blinking.
Same cable used to connect between network switch and PLC connected to my laptop from PLC eth port and pinged, its communicating. What is the reason for this?? Can i get a Solution from anyone??

Hi,
please check if you are using a “normal” patch cable and NOT a cross-over cable.

Stephan

The cable should be irrelevant in this case as the C80 does support Auto MDI/MDIX
When connecting a switch or hub to the Ethernet port of the C80 the link should work without any issue.
Have you checked if you use the Ethernet port or did you accidentially use the Powerlink port ?

1 Like

i tried same connection with cable i used to transfer program. that time also same.

Connected in ETH Port

The cable you used to transfer the program ? So you already transferred over Ethernet ?

Are you using a managed or unmanaged switch?

1 Like

Hi,

does the switch have 2 LEDs, often called “link” and “act” (activity)?
And

  • if “yes”, are both LEDs off? Or is the “link” LED on, but “act” doesn’t flash?
  • if “no” (only one LED), is this LED off or permanently on (no blinking)?

I’m asking, because normally switch LEDs are indicating 2 different states:
1.) the physical link state on layer 1 (is a ethernet connection detected?)
2.) the layer 2 communication state (if packets are going through the port, a combined LED, or, in case of two LEDs, the “act” LED is blinking)

The physical link state is detected by simple voltage pulses, without layer 2 data transfer (auto negotiation, so the detection of the cable type and the communication speed, is part of this layer 1 procedure).
The activity LED, or the flashing of a combined LED, signals that layer 2 data is transferred (most often, only if data is received by the switch port), so the 2 devices are communicating.

If 1.) fails, most often the cause is some defective cable or interface, or the auto-neg procedure fails for whatever reason (for example because of some fixed speed settings in one or both devices, that don’t match).

If 2.) fails, one reason could be that the switch “want’s to see some incoming data on it’s interface” first, to learn the physical address of the device behind (the MAC address), or some filters / setup inside the switch prohibits the data transmission… in such a case, it can be helpful to “force” some outgoing data from the device to the switch, in our case for example by sending a ping from the PLC to some other device (it’s not neccessary that the ping receiver really exists, but sending a ping from the PLC will end up in a layer 2 packet sent to the switch).
Of course the’re many other possibilities why the layer 2 communication could fail, especially if it’s a managed or a “smart” switch.

Best regards!

1 Like

Yes, i already transferred through ETH. When im trying to establish connection through switch only its happening. Can connect directly to PC and communicate with PLC through ETH.

using unmanaged Switch

Im using unmanaged switch, both LEDs are not blinking. While pinging packets Sent:4 and Recieved:3.

Ok, now I’m confused: I understood that the communication with the PLC isn’t possible at all, but you’re receiving ping responses?
Are more devices connected to the switch then the PLC and the notebook, is there maybe a IP address conflict (another device uses the same IP address as the PLC)?

I know I am pulling straws here but

  • Did you try a different port on the switch?
  • Did you try a different cable?
  • Did you try a different switch?

All three ways tried

Hello, Aswin
It is quite unexpected that such a problem is still not resolved after more than 1 month and a lot of efforts from the best members of this community.
It seems like we are missing some critical piece of the information. So, could you please answer EACH of the following questions in AS MUCH DETAIL as possible?
(please do not give us just a simple one-line reply…)

  1. We are assuming that you are using 2 (two) good quality normal Ethernet cables (Cat5E or better, with RJ45 connectors on both ends) connected between your notebook (PC), unmanaged L2 switch and the ETH port of the C80 device (PLC).
    Is our understanding correct?

  2. Are there are any other network devices connected to the same L2 switch?
    (if so, please disconnect ALL of them, at least temporarily)

  3. Assuming that “Port 1” of the switch is connected to the notebook (PC). Do you see 2 LEDs active?
    (one should is steady ON, indicating a “link” and another one is blinking at some rate indicating a data transfer)

  4. Assuming that “Port 2” of the switch is connected to the ETH port of the C80 (PLC). Do you see 2 LEDs active? (as described above)

  5. If the answers to both questions #4 and 5 are YES, please provide us with information about the IP address and netmask of both notebook (PC) and the C80 device (PLC).

  6. Can you ping the C80 device’s IP from your notebook?
    (use “ping -t” command to send an unlimited number of pings; interrupt withCtrl-C)

  7. What is the success rate of the pings ?

  8. Launch Automation Studio, open the project which has been loaded into the C80 device and send us a full screenshot with at least the following details:
    a) Online Browse" view of a Ethernet network
    b) bottom status bar which shows the device model name and its status (RUN, SERV, etc)

Well, I hope after getting your detailed answers to all of these questions we can come up with some suggestions and hopefully solve the problem! :handshake:

Thanks and Best Regards,
Alexander

1 Like

closed due to inactivity