how do I calibrate the touch screen on a power panel 400 that uses Linux OS?
Good afternoon @arijaluddin,
To calibrate a touch screen, it is necessary to program a button on the HMI.
If this button does not exist, the only possible way to recalibrate the screen is to generate a new Compact flash including this button.
If this PP400 uses Automation Runtime and VC4 Visual Components, the developer has two possibilities to provide touch calibration:
- using the key action Calibrate Touch
- using the VISAPI function VA_StartTouchCal
I hope this helps you!
so have to recreate the program that includes a button for touch calibration?
I’m sorry but I am not aware that there is another option to achieve this, so yes, this would be the way.
oke thanks for your help sir