PC3100 + Panel SLD4 but no touch work

Hello community,

I just started a PC3100 with a panel and an SLD4 interface. The PC start normally with windows, I can use a mouse and a keyboard connected on the screen… But the Touch don’t work … I touch the screen with my finger but nothing …

In the menu of windows, under the B&R Automation, I don’t have the program “Touch screen settings”… But on an older PC3100 I had few month ago I had this program …

Have you an idea how I can install the touch screen function ?

Thanks in advance

Hello,
some Questions:

  • which panel are you using?
  • how is APC3100 conntected to Automation Panel SDL4 Receiver (via SDL4 converter or SDL4 transmitter?)
  • which Windows is running on APC3100

BR Andy

I had a similar issue with the touch intermittently working. The suggested fix was to update the panel to the newest firmware but that didn’t seem to fix it. However assigning the USB ports on the SDL4 interface on the panel to the GPOS fixed the issue for me.

Panel : 5AP1120.156B-000
SLD4 Transmitter 5ACCLI02.SD40-000
Windows 10 IoT Ent 2021

5AP1120.156B-000 is an singletouch Panel. In that case the Touchdata are transfered via COM Port.
For Singletouch Displays B&R offers an Singletouchdriver- see Touch Treiber B&R (WinXP, Win7, Win8.1, Win10 32/64-Bit) | B&R Industrial Automation (br-automation.com)
With that you also will have the “Touch screen Settings” you mentoined…

Additionaly it could be, that you also have to enable corresponding COM-Port in BIOS…

The Information regarding COM Port you will find in APC3100 User Manuel ( MAAPC3100-ENG_V2.16.pdf (br-automation.com)) at Page 151. COM A is the SDL onboard touch screen Port- so this Port has to be enabled in BIOS (Setup Utility → Advanced → OEM Features → Super IO → COM A).

If you are Using SDL4 Transmitter it should be COM E according to Informations at Page 51 and 152.

Thanks a lot … with this driver all works fine …
In the bios, the SLD was already enabled …

Thanks for your solution, but I had just not the touch driver installed on the windows.

Best regards