Touch Lock Driver not working

I have an APC910 that connected to 2 panels - 5AP99D.215C-K.
The IPC used to be in Win7 and was recently upgraded to Win10 32 bit. After that the touch lock function is not working. Under the control center, the panel status still changed from lock<->unlock and vice versa but the physical touch is not disable when panel in locked mode. The installed touch lock is V1.3.0 and i noticed that Win10 32bit support is removed under the change note. I couldn’t found the older version on B&R website, anyone know if V1.2 will work on Win10 32 bit and where is the download link?

Hello and welcome to the Community,

The Touch Lock driver for Automation Panel 9xD, supported in Windows 10, is available here (login required).

Hi, the link only listed V1.3.0, do you know where can i get the V1.2?

Hello,

Please contact local B&R support. The “lock<->unlock” issue should be investigated in more detail, and they could provide you with the V1.2 driver if that was a potential solution.