On‑site setup: APC910 controller connected to two 5AP1130.185C‑000 touch panels via SDL4. Dual‑screen interlock function is required.
Touchlock driver installs and works normally on all previous projects. However on this project, one panel fails to start the touchlock driver after installation.
The panel itself has fully functional touch, all other drivers install without issues, only touchlock fails.
The serial number of the problematic M0 panel and the HMI report are both attached.
Most likely there is some kind of a incompatibility with the Touch Lock driver.
You could try with the most recent version of Touch Lock and if that does not work please report this through the official support channel for your country.
I have tried every publicly‑available TouchLock driver from the B&R official website, including the most recent release.
All of these driver packages were published prior to the M0 screen revision dated 03/26/2026. Unfortunately none of them can take effect on this M0‑revision touch panel.
Could you please advise whether there is a new TouchLock driver built specifically for Revision M0 hardware?
If a dedicated driver is not yet publicly released, are there any feasible workarounds to fix the compatibility problem using existing older drivers?