Calling OPC UA server Method using UaExpert

Hello,

I am using opa-ua server on a C30 panel.

For future uses, I want to create some features, something like acknowledge one alarm or all alarms using methods.

For test, I created a Method and enabled the tag on opcuaMap.uad
image

My program looks like this (quite simple):

VAR
    opcua_Method_AcknowledgeAll : BOOL; 
END_VAR

PROGRAM _CYCLIC
    (* gb_MpAlarmXListUIConnectType.AcknowledgeAll is a global PV
         it is used to create a connection between MpAlarmXListUI and the HMI application*)
    gb_MpAlarmXListUIConnectType.AcknowledgeAll := opcua_Method_AcknowledgeAll;
    opcua_Method_AcknowledgeAll := FALSE;
END_PROGRAM

When I call the method using UaExpert, I get this Error.

In the other hand, when I force the PV opcua_Method_AcknowledgeAll to TRUE directly in UaExpert, it works and all alarms are acknowledged !
image

Do you have an idea to overcome this issue ?

I have one more question that can be out of this topic. Does opc ua on B&R panels support file transfer (OPC 10000-20: UA Part 20: File Transfer) ?

Thank you

Best regards
Mohammed Ali

Hi Mohammed,

A Method in OpcUa is essentially a function, running on the Server and callable by Clients. It has inputs and outputs. When a client calls a method, the server runs some code and then returns the result.

The way I read your post, it sounds like you’re just looking to read the value of a variable. In this case, you do not need a method. You can use the OpcUa Default View (.uad) file to expose a boolean variable over the network, and then set that variable with your client. Note that your client must also reset the variable in this case.

If you want to use a method, you need to:

  1. Define the method within a program using the Methods (.uam) file
  2. Expose the method to clients using the Default View (.uad) file
  3. Use the UaSrv_MethodOperate function block in the AsOpcUas library to check that the method has been called, and then let the client know that the execution was successful after the method has been run.
  4. Run your function or action when the UaSrv_MethodOperate function block indicates that a client has called your method, and then return the resulting output.

You’re probably getting that timeout error because, without the UaSrv_MethodOperate block running, your client doesn’t know that the method has been run.

I’m not sure about your second question. I know that file transfer with B&R devices is possible (using FTP for example), but I have not done it using OpcUa before.

Hello Marcus,

Thank you for your quick answer.
Indeed, it seems that I did NOT understand the use of methods. I gave the example of AcknowledgeAll alarms just to understand and test methods. I am planning to use them in more complex functions.

Even if the question has already been answered in principle, there are other topics in this context that may be relevant in the future.

If a method call is made from the client to the server, the call can be checked with the UaSrv_MethodOperate function block in the application. However, this only checks whether the method has been called but it gives no no feedback to the client, wether the call has been recognised and is being processed.
The client only waits for feedback from the method call in the form of the finish-command, which must be set via the function block.

This can result in a timeout for methods that have longer processes (ex. moving an axis to a specific position) and the finish is therefore only set after some time.
A timeout is therefore only defined on the client side and must be set there.

With UaExpert, for example, this timeout can be set via a global setting value.