Clone B&R Panel PC 2100 CFast Card

With PVI Transfer you have to use .zp3 image, because for .zp2 image the same card type has to be used. You could also look at other image tools like HDClone.
See also this thread:
Compact Flash(CF) or CFast Card Back Up and Health Checking - Share Info & Ideas - B&R Community
If the card contains Windows 10 iot 2015 than the cloned card could not work, because of the hardware change can disable the windows activation code.

The image tools must be smart and not a bit for bit copy.
If Windows 10 iot is used it is always smart to do a retrim on the cloned card.