Did anybody already tried to make connection to Siemens PLC with DavNoDave library?
Just adding the library into the project creates 2500 errors.
Working example would be appreciated. X20 PLC to S7-300.
I don’t have it, but I imported the library to AS4.12 and restored the sample task and configuration file from the documentation. Maybe this will help you. ISOTCP_AS412.zip (190.6 KB)
Hello! I am sharing a working apllication where X20 PLC data shared between S7-300 PLC. Thank you all for help! X201584toS7300.zip (285.6 KB)
PS:The only thing missing is to make it work also to S7-1200, which is currently not working, although connection is established. So, if there is someone who would make an idea why not, I would appreciate the hints.
Thank you @tommi.piiparinen, I knew that before that I need to disable it, but somehow it didn’t work. When I went again everything through step by step, it started to work. So, application is now working.
Just to mention, my main idea behind this excercises it to offer a B&R PLC next to an existing Siemens PLC and create mapp View visualization for the machine to be accessible from the WEB. Without touching installed and working Siemens (S7-300 and S7-1200).