Connect X20 DC Module X20DC1376 with ACOPOS P3 drive

I want to connect X20 DC Module X20DC1376 with ACOPOS P3 drive and as per Received Encoder signal (from different motor), I want to synchronize Main motor with new ACOPOS P3 connected motor.

Is it possible to connect X20DC1376 with ACOPOS P3 drive and share ParID for Speed and all parameters.\

Hello,

I am not sure if i understood your UseCase in a correct way…

1. PureVAx - DC-Module as External Encoder
You can use a Purely Virtual Axis - With the Mode “External Encoder” to Provide
the Data of the DC-Module to a Axis Object, which can then be used as a Source for Axis Coupling.

2. Network Encoder on ACOPOS P3
You can SetUp an Network Encoder on an ACOPOS and Transfer required Data via CyclicParID. This Network Encoder can also be used in the context of Motion.

Network Encoder on P3

If you only need the Virtual Encoder for an External Encoder, you can use the Settings in ACOPOS P3 Konfiguration.

Greetings
Michael

hi @Akshay_Chavan is it your issue solved, can you update us?

Hello @Jaroslav Kovar, Currently, it is under implementation, Customer is waiting for hardware, once hardware will be reach at customer site, we will test and let you know.

Please use this channel for your update, so we can mark it as a solution :slight_smile: thanks