Data Transfer between DTEL and B&R via ETH/IP

I want to create a data transfer and communication between DTEL and my Machine via ETH/IP. I am using 5ppc2200 Controller. Please guide me through the process.

Hello,

first you need to clearify if B&R is the master or slave. Depending on this you can then select the necessary hardware.
As the PPC2200 cannot handle PCI cards you would at least need a PLK interface and a X20BC1083 where you then plug:

  1. A X20IF10D1-1 EthernetIP Scanner (Master) or
  2. a X20IF10D3-1 EthernetIP Adaper (Slave)

In general you import an EDS file in the masters software which describes the slave and let you select data which is exchanged

Lets assume the B&R PLC is the master.
This would mean you have to have a PLK interface in your PPC2200 with a X20BC1083 and plugged X20IF10D1-1
You then need an EDS file of the “DTEL” device which is imported in Automation Studio.
The hardware will then be available to “drag and drop” in our hardware tree

This could look like this:

Dear Oliver
Thank you so much for the information.

You are very welcome !