DATE_AND_TIME 64bits / OPCUA

Hello,

does B&R supports DATE_AND_TIME 64 bits format?

Is there any function to convert from 32bits to 64bits format?

I value shoud be send through OPCUA and it needs to be linked to an external information model object. The object supprts only the 64bits format.

Thank you!

Not directly, but you can get the DateTime information into a variable of structure type, which contains 2 DINT variables.

UA Part 6: Mappings - 5.1.2 Built-in Types

In the OPC UA Default view in the UA Data Type column the i=13 DateTime can be used to get the INT64 into 2 DINT values.

It works perfectly. Thank you!