Hello all,
I am facing an issue at customer where I am getting an error “28850 - Invalid Device” for serial port I want to use in PLC.
Below is the image which shows the Physical configuration, I am communicating variables on serial port RS232. I have added variour device names like ‘IF1’, ‘SU1.IF1’, ‘SL0.IF1’, ‘SL0.SS1.IF1’, ‘SL0.SS0.HW’ but for all of these I am getting the similar error for getting node data.
PLC: X20CP0410
Serial: IF1
So, I wanted to know that how getNodeData function block for AsHW works, and what other configurations I need to look for and how the device name should be given for the same.
Serial parameters like BD, Parity etc is configured Ok.
Hope for the response soon.