Hi in a program done in V4 i was able to assign an enumeration to a BOOL[0..31]
but in v6 it’s not working anymore

![]()
Can you help me to solve this problem?
It does compile, but the project can’t run once loaded in a PLC.
Hi again,
I tested it today. My Dummyproject does run on a PLC with 6.1. No warnings, no errors. Even the powerflow is working for other networks, after setting up the OPC UA connection ![]()
Still the erroneous network is causing issues from a viewing perspective.
Maybe the there something in the logger indicating what the issue is, I doubt that it is just because of the network.
BR Fabian
Hello @fabian.pries
A customer has the same problem, have you found a solution?
Thank you
Hello @grifl,
I did not find a solution, but to be honest I did not search for one either.
It seems like an issue with the view of the editor but not a functional issue.
You might want contact local B&R support to clarify the behavior of the editor.
BR Fabian