Error: mcCOMM_STATE_NOT_ACTIVE

Hello, my problem has been solved. Thank you, but this time I’m getting this error code -1064239101 mcCOMM_STATE_NOT_ACTIVE

That sounds like an invalid MpLink input. Check the function block that’s giving you that error. Are you passing the correct MpLink to that function block? Are you passing the correct format (usually a pointer to the MpLink rather than the MpLink itself)?

I matched it correctly; I did this using the adr command.

That error number is used in multiple libraries, and each instance has something to do with an invalid MpLink input. That is the best I can give you without more information. If you want help from the Community, you’re going to have to tell us more about your project and the context surrounding the error, such as:

  • Which function block is this error occuring on?
  • Which mapp Link are you using? What type of mapp component is it?
  • Are there any errors related to this mapp component or the function block in the Logger?

Moderator note: I’m going to unlist this post until more information is provided. There is not much anyone can do to help with what we have now.

CLosed due to inactivity of author.

As far as I understand, the acp10 libraries had been left inside cpu.sw and were causing a conflict. The problem has been resolved.

Thanks for updating us!