EtherCat with mapp motion

can we please have a demo program with the setup for a basic motion axis using an ethercat servo

Hello,

A Ethercat Servo is a 3rd Party device and i do not have a Description File for such a motor at hand. But i know that it is intended to use a PureVirtualAxis with GeneralPurposeAxisInterface Mode DS402 for this UseCase.

Here the Documentation in AS-Help:
DS402 CSP - Cyclic synchronous position

In General you have to create:

  1. Axis-Configuration Object

  2. PureVirtualAxis-Configuration Object
    image

  3. Link both objects by the Axis Reference

  4. Create a Variable Structure which Contains Variables for the DS402 Interface

  5. Link the Variables to the PureVirtualAxis-Configuration

  6. Link the Variables to your 3rd Party Field Bus ethercat servo

  7. Setup Mapp Cockpit

Follow up with the Testing.

Greetings
Michael

hi Michael thank you , during this time iv managed to get everything working

Hello,
I am happy to read this.
If you like you can share some Screenshots as a Guide for others aswell, if you like.
Was there a special “stepping stone” you had to overcome which was maybe difficult to find in the Help?

Greetings
Michael

happy that it is working, would be great if you share with us some details.either here or as a regular new post in Share Info category. THanks a loooot in advnace :slight_smile:

Hi Guys,no problem will

Upload soon