Hi Marcus,
thank you for that information.
But this was a question, which i was asking a long time ago.
Now I have the problem that i got no communication with the plc CP0483.
I can see at my wireshark program the plc with the ip 10.254.106.131 (picture above).
Problem is i got no response. It happend at the last program download to the plc.
I was asking if there exists a option for factory reset manually.
![]()
Freundliche Grüße / Best regards
Franz Christian Wilhelm
Elektroanlagenbau / Bauleitung