Hello,
I’m using the FTP server on an EM0612 CPU, Runtime version 6.3.4, with a C# backend using FluentFTP. The backend places the files in a folder on the FTP server. I copy this folder on the FTP server and read the files in the copied folder using FileIO FBs. Sometimes the files become corrupted and can no longer be opened (neither with FileZilla nor WinSCP, nor via the FileIO blocks). The corrupted file is located in the folder where the backend stores the file; however, it is fine in the backend itself. Furthermore, part of the content of the corrupted file appears in another file on the FTP server. No FileWrite is called either. The folder containing the corrupted file can be copied using DirCopy, but the file in the copied folder is then empty.
In System Diagnostics Manager, it appears as though the partition has been damaged.
Has anybody a solution for this?
kind regards
Oliver