Generating project installation package using command line

Hello,

I would like to know if there is a way to create Project Installation Package via cmd prompt (USB installation package).
I couln’t find the appropriate command on the “C:\BrAutomation\AS412\bin-en”

Thank you,

Hello,
I do not believe there is any direct command operation to create a PIP.
What is your goal?
The Runtime Utility Center package may be of some help.

This is not possible directly, Runtime Utility Center is required as an extra step.

This message and the whole thread should include useful information. A bit different usecase, but using RUC to create a PIP package instead of ArSim instance does the trick.

here is the description of just BR.AS.RUCPackageCreator.exe:

B&R Online Help

Hello,

@david.nytko We use USB stick to update the program on PLC. In my project, I have 3 configurations, I tought it will be easier to automate the creation of the Packages.

I will dig into using Runtime Utility Center. Never used it before, but i will use the docs provided by @tommi.piiparinen and @christoph.hilchenbac

Thank you all,