Automation Studio API

Hi Community,

Quick question here. Is there a way to automate some of the operations in Automation Studio?

I’m looking for a similar thing of SIEMENS TIA Openness that allows a way to perform some tasks with an application via the API, so we don’t need to manually do it.

This will be very useful when it comes to update multiple PLC programs for sites.

Thank you for your help.

Hello.

As the project files are text files you can use external scripts (batch, python…) to modify the project pretty much as you wish.

Combine the project modifications with the command line interfaces of Automation Studio to build and RUC to transfer and you should be good to go.
Automation Help: Build project using command line

Using these it is possible to create a complete CI/CD pipeline, BnR-DevOps-Package can help with this.

Hi Tommi,

Thank you very much for your information, I will dig into this.

Hi Tommi,

It’s been a while.

Thank you for pointing me to the information, it was very helpful.

Is it possible to include unit test? It seems we need to run a ARSim instance that hosts the unit test. Can you point me to some information about how to integrate the unit test in the pipeline, please?

Thank you for your help :+1:

Hello,

You are correct that an ARSim instance is needed. RUC can spin this up for you.

I have used a separate “UnitTesting” configuration in Automation Studio for this and I first build a RUC package for this unit testing configuration, then i use RUC to start the ARSim instance and then it is possible to run the unit tests with HTTP requests. I used a powershell script to run the tests and parse the results so that I could return either a pass or fail value.

Automation Help: Using the Unit Test web service

Here are some commands, which might be helpful. (I have used these with GitHub actions). Replace the <> parts with relevant informations for your project.

  1. Create RUC Package for Unit Test configuration, force simulation
C:\BRAutomation\AS412\bin-en\BR.AS.Build.exe "<PathToProject>/Project.apj" -c <UnitTestConfigName> -buildRUCPackage -simulation
  1. Create a instruction list(PIL file) for PVITransfer (RUC)
Write-Output 'CreateARsimStructure "<PathTo>\RUCPackage.zip", "<Path to where you want to create the simulation>", "Start=1"' | Out-File <Path where you want to create the pil file>\CreateUniteTestArsim.pil -Encoding ASCII
  1. Create and start ArSim
Start-Process -FilePath 'C:\BRAutomation\PVI\V4.12\PVI\Tools\PVITransfer\PVITransfer.exe' -ArgumentList '-silent -<Path to PIL File here> -<Path to log file>'

I see, thank you Tommi. It is very helpful :+1:

Hi together,

maybe it is right that you can change all textfiles in the background to configure your project. But what is about passwords (e.g. in the usermanagement). I want to change the passwords automatic. But the passwords are hashed with an salt, that I didn’t know and only the hash is saved. Is there any option to generate the passwords automatic?

Regards
Jan

Hello @tommi.piiparinen

I cannot find anymore in AS6 the command “CreateARsimStructure”

Do you know how it has been replaced? or is there a workaround to Create and start ArSim?

Thanks

Marco Sartori

Hello Marco,

In RUC/PVI6 the command has been renamed/modified a bit. It is now part of the “OfflineCommissioning” command, example below. (You can also use RUC to graphically create the command for you.)

OfflineCommissioning  "<PathTo>\RUCPackage.zip", "ARSim", "DestinationDirectory='<Path to where you want to create the simulation>'", "Start=1"

Automation Help: RUC OfflineCommissioning Command