- Move all licenses from the TG to the server.
- Plug the TG on a PC with AS
- Start Codemeter Command Prompt: Start → All programs → CodeMeter → Tools → CodeMeter Command Prompt
- Enter the following command:
cmu32 /l
- Record the SN from the TG
- Enter the following command:
HID
cmu32 /s x-xxxxxxx --set-config-disk HidCommunication
MSD
cmu32 /s x-xxxxxxx --set-config-disk MsdCommunication
here you have to change x-xxxxxxx to your serial number (e.g.: 2-1234567).
- After finishing un- and replug the TG
- Move the licenses from the server to the TG

The printing on the TG dongle shows if it is an MSD or HID from the factory.
- 2-* MSD
- 3-* HID