I can not run endat2.1 8BAC0120.000-1 modul

Hello ;
There is a old machine and I try to replace Panel PC with 5PPC2200 but there is a problem acopos multi system.There is a physical endat2.1 module on driver.


When I add endat2.1 IF module config

to driver SDM show me warning

When delete to plug on driver sdm is ok no problem.


I have no ideat about it.Could it be a version problem or something?

AS version is 4.12.2.93.

Could you please explain a bit more, what you have changed and why?
Did you change the software? Or did you change the PC against the same PC and use the same CFast Card?
Beside the warning in the SDM, do you get more error messages?

Due to inactivity marked as a solved.