I get the Error -1067352607 and dont know what to do

Hello there,
I’m relatively new to programming SPS modules so please forgive me if this solution is to obvious.

I got two systems: the ETAL310.1C05-1 and the ETAL410.1033-1. The first one is running without an issue, so I wanted to set up the second one. Since the ACOPOS-Micro in the second system, has no CPU, I connected it via PowerLink with the CPU from the first system (4PPC70.0573-20B). So far so easy.

After setting up the ACOPOS with two axes, getting all the settings ready and writing a little test-program, no matter what i try, I get this error and I don’t know how to solve it.
Im currently running AS: 4.12.6, AR: J4.93 and MM: 5.28.3

Is there any specific setting i have to change ? Do i have to use an other AR version ?
SDM says its not even plugged in but i obviously have.

I hope you guys can help me out.
Regards, Moritz
grafik

Hello,

i work a lot with B&R Motion but, as far as i remember i never had this error.
The AS-Help “Casue and remedy” section talks about rebuilding the Project and about Versions.

Can you check that you have the Library McAcpAx in your Project and assigned to the plc (Software Configuration)

In this Guide there are all Steps for a generall Commissioning descriped. The base for this Guide was the ETAL410.1033-1.

Guide Motion Comissioning for beginners

I think based on your Odernumber you have the Resolver Option on your Motors .R0
The ETAL was also available with .B1 Encoder Option so for all who are using B1:
In this Thread there is the B1 Encoder Option descriped.

8LVAxx.B1 EIB Encoder ParID 719 → 1

Greetings
Michael

Thank you really much for your answer! I found the mistake, there were incorrect settings in the PKL and 80VD100.. Configurations for Controlled and Managing Node.

Now the system is running.

Since you also used the ETAL410.1033-1 in your motion guide, can you tell me, if you used it in your single and multi axis guides? In specific, if i want to run both motors simultaneously, can i use MpAxisBasic two times and give each one an axis and a AxisParameters reference, or do i have to use axis groups and MappRobotics, even though the axis are in no correlation to each other?

You can use two instances of MpAxisBasic and AxisParameters references to have two independent axes.

Hello,
I may add that also in a situation were you use an AxesGroup for GroupCommands its often usefull to have a MpAxisBasic instance for each axis, to allow single Axis commands for service purpose in the application.

So i would typicaly say that it is most common to have a MpAxisBasic Instance per Axis.

Greetings
Michael

Hello,

Do you have the original source code of two Kits? Would you mid send them to me?

Thanks,

Tung