Install APROL R4.4-01 on VM nested configuration, run AprolConfig with error QFDN hostname

Dear All,
Install APROL R4.4-01 on VM nested, run AprolConfig with Error: FQDN hostname
I tried to install APROL R4.4-01 on VM(conf 8x vCPU, 8GB vRAM, 260GB vHDD, 2x VMX Net3), installation did successful but running AprolConfig with error QFDN hostname. Please let me know what happened to me. See attached for my error

Thanks
hatien

you need to configure the hostname in Ethernet settings as fully qualified hostname, means including domain / DNS suffix

Thanks! I must change in /etc/hosts for the 127.0.0.2 example.adomain example. It is OK but the next step I faced many problems with LDAP and license license 90 days. I did go back to APROL R4.2-07.

If you configure with yast there should not be anything to do manually in the hosts file.
Yes there are a few things new in R4.4-01 but if you follow the documentation you should be fine.

Could you support this again, i only install and configure APROL standalone(engineering/runtime/operator) on the same Control Computer. The different Operator between Net Operator(by VNC), they are the same or actually different?

Thanks
HTT

The operator system is a linux user.
In general, it doesn’t matter if you use it locally or via VNC (or other remote services).

To answer your question; it’s the same.

Dear Ha Tien,

I am also running APROL 4.4-01 on a VM with AutoYaSt SLES 15 SP6. I would appreciate it if you could share your experience with setting up the LDAP server on APROL 4.4-01. I always get an error importing a specific tmp.ldif file and I dont really know the reason why. The 389 DS package is installed and I cant find a solution in the documentation.

thank you in advance for your reply!

Dea Mohamed Aly,

I already went back to APROL R4.2-7.

Regards,
hatien