Is it possible to use modbus to control P74 inverter?

Hello everyone:
I have a P74 inverter model 8I74T400075.010-1. There are some questions I would like to ask.

Question 1: There is a modbus interface on this inverter with an RJ45 connector, and I see the following wires in the manual. I would like to know if this wire is network based or serial 485 or 232?

Question 2: Can I use modbus communication to control this inverter? Or is there any other external IO for control? Is there a more detailed manual available.

Any help is much appreciated!

Hello

Forget about it. The cabe is a custom cable used to configure the safe functions of the ACOPOSinverter P74/P76 via the software SafeConfigurator.

B&R Online Help (br-automation.com)

Thanks, very helpful.